All_PCU_Core_V4.1_DCDC_2.pdfAll_PCU_Core_V4.1_DCDC_1.pdfAll_PCU_Core_V4.1_DCDC_3.pdfAll_PCU_Core_V4.1_DCDC_4.pdfAll_PCU_Core_V4.1_DCDC_5.pdfAll_PCU_Core_V4.1_DCDC_6.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Xiaofu,
Can you provide the PCB source file of LM5116 section? or provide print file as below:
1. Top overlay+Top layer
2. Bottom overlay+Bottom layer
3. Bottom layer+top layer.
B R
Andy
Hi,
Pls modify the circuit as attached
On the layout:
C91 position for IC is good
C92 position for HS LS FET is bad
VCC cap C68 was not placed close to IC, and short GND plane with multi vias.
B R
Andy
Can customer test board temp close to LM5116?
Keep VCCX cap 1uF, connect Vout 12V to VCCX pin, check if the IC temp will reduce?