Part Number: TL431
We are currently using TL431AQDCKR.
We are considering changing the Vref tolerance from grade A (1%) to grade B (0.5%).
We have a question about this.
[question]
We think that the only characteristic change due to Vref grade change is the Vref tolerance,
and there is no other characteristic change.
Is this understanding correct?
If there are any points to be noted in addition to the change in the Vref tolerance when changing Vref grades,
it would be greatly appreciated if you could give us some advice.
Best regards.
Toru