Hi Team,
may customer is looking for an alternative part for PCA9624:
requirements:
- 8 channels PWM
- I2C
- min 50mA Iout per channel
- Supply Voltage >=27V
If no part available also lower channel count can be considered.
Thanks
Jan
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
may customer is looking for an alternative part for PCA9624:
requirements:
If no part available also lower channel count can be considered.
Thanks
Jan
Hi Hardy,
Can you find out how dramatic it would be if the 27V is applied to the output pins instead of the 17V or max. 20V would also be possible?
Would this lead to a destruction of the pins?
Possibly one could protect the outputs by means of Z-diode, which is however no beautiful solution, since thereby a permanent basic current develops.
Therefore it would be interesting for me, what happens if the output pins get a voltage >20V.