Part Number: TPS62665
Other Parts Discussed in Thread: TPS62660,
Hello,
From the datasheet, it is mentioned that the converter is optimized to operate with 0.3uH - 1.3uH inductor and 4.7uF - 10uF output capacitors. 
Would like to know if there is a max allowable output capacitance for the controller to achieve stability or if there's any requirement on the output capacitance with this controller? Reason being is that the effective output capacitance on my board is about 47uF. There is a 4.7uF and 10uF near the controller side while the rest of the different combination of capacitors are scattered around the load side. The inductor used is 1uH in this case. I understand that this can be verified on the board by looking at the jitter, oscillation, transient response and etc, but it would be good if I can have a rough idea in designing phase whether if it is affecting the current design.
Besides, looks like TPS62665/TPS62660 is not available in TI Webench and library in PSpice for TI. Thus, I couldn't do a simulation to confirm whether my design is fine. Is it possible if these parts can be added into any of the simulators above?
Appreciate your support in advanced. Thanks.
Regards,
Kean Leng