Hi,
My customer is evaluating UCC27537 and have some concern about the Input signal threshold. From the table we can see the Vin_H(min) = 1.8 V and Vin_L(max)=1.2V. So in the worst case the input signal hysteresis is only about 0.6V. In some case of huge input ripple it may cause the misreading of the input status. Are there any solution for this or 0.6V is enough for the input signal hysteresis ?