This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS23755:RSRF, RSRR rated power and transformer

Part Number: TPS23755


Dear Team

I have two questions.

① Is the rated power of RSRF and RSRR 1 / 16W sufficient? I don't think it needs a large rated power because it drives the FET Gate.

② When asked about alternative transformers, you answer, "The two recommended transformers are specially designed."
  What are the specific characteristics of them?
  Detailed information is needed to select a replacement.

Thanks in advance