Hi,
I have problem in using TPS71933 IC, I need 3.3V at different times for 2 different channels. My input power supply is 5V and my controlelr needs 3.3V. So i started using TPS71933, Intially it worked fine TPS71933 provided regulated voltage 3.3 at the output of it. Later though it produces it is consuming more power and hanging my system from working.
Initially total system used to consume 8mA current (every module working). Nowthat, it started consuming 15mA and no device works in the circuit. If I detach a TPS71933 IC and provide 3.3V to my circuit individually it works fine. What am I supposed to do with the TPS, I have clearly checked there in no continuity problem assaosiated with the TPS IC. Please suggest me what went wrong.