This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63802: For insufficient VOUT discharge when VIN=0V

Part Number: TPS63802

Hello, 

Is it acceptable that VOUT is not completely discharged when VIN=0V (EN=floating) in TPS63802?

If the power supply is turned off because the load on the VOUT side is small, VIN = 0V, VOUT = 0.9V, and VOUT is gradually discharged.
It takes about 1 minute for VOUT to be completely discharged.


Also, does the IVP function work in this state?
I do not need the IVP function in my system.

Thank you in advance,