This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25710: For insufficient VSYS discharge when VBUS=0V and battery not connected

Part Number: BQ25710

hello,

With the battery unconnected, the AC adapter is used to power the system via VSYS.

There will then be some voltage remaining in VSYS when the AC adapter is removed. (0.6V)

Is it acceptable for a charge (0.6V) to remain on the VSYS terminals when the AC adapter is not connected (VBUS=0V) and the battery is not connected?

We are concerned about whether the BQ25710 will malfunction or fail if a charge remains on VSYS when the supply power is completely disconnected for our system.

Best regards,