This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ24770: AC mode

Part Number: BQ24770


Hi team,

Does the bq24770 have a register to directly determine whether the AC adapter is plugged or unplugged? Thanks

Best regards,

Sam Ting

  • Hi Sam,

     

    For BQ24770, there is no register that can be read back to indicate AC Adaptor status. AC Adaptor status is indicated by ACOK pin.

     

    ACOK is pulled HIGH to external pull-up supply rail by external pull-up resistor when a valid adapter is present (ACDET above 2.4 V, VCC above UVLO but below ACOV and VCC above BAT). If any of the above conditions is not valid, ACOK is pulled LOW by internal MOSFET. Connect a 10- kΩ pull up resistor from ACOK to the pull-up supply rail.

     

    Thanks,

    Khalid