Other Parts Discussed in Thread: BQ79616
Hello
we got some issues with connection of battery pack with BMS configured with three stacked BQ76PL356 front ends in following configuration: 6/5/3 cells (in sum 14S configuration). Actually the connection order is BAT_MINUS --> Top_Cell --> Cell1_to_13. All cells and input are protected with 5.2V Z-Diodes.
Somewhere in connection process the top front end with 3 cells gots defect and drwas significant current from the top three cells even in sleep mode. All measurements and communication is running well.
I am aware that the recommended connection order is from bottom to top, nevertheless I would like to understand what could went wrong with this oder. Is there any protection diode inside the front end which could get broken in plugging moment? Is there any issue when working only with three cells on one front end?
Thanks
Torsten