Other Parts Discussed in Thread: BQ20Z70, , BQ40Z50, BQ20Z80
Hi,
For one of our customers, we have re-designed a long running legacy battery product from a BQ20z70 to a BQ40z50-R1.
Due to the backward compatibility required between the old and new battery packs as far as Battery Status registers are concerned, the TCA bit in Battery Status needs to remain set even after the charging has stopped and the average current is zero.
In the BQ20z70, this is possible and the TCA bit remains set, along with the FC bit. However, I have not been able to achieve this with the BQ40z50-R1, as the TCA bit changes to zero once the average current drops to 0.
I have tried all the options within SOC Flag Config A and SOC Flag Config B.
Please can you assist?
BTW, I did see a 5 year old thread on the forum where Onyx implied to a query that in the BQ40z50, the TCA bit will always revert back to 0 soon after being set, but it was not clear to me if this was to a particular GG file or it is a change designed into the BQ40z50 over the BQ20zXX fuel gauges.
Thanks and regards,
Zahid