Part Number: LP8733
Hi team,
Could you help me to check if my understanding of LP873345 soft-start is correct?
From datasheet p. 23-25,
1. Both DC-DC and LDO have soft-start
2. In case of DC-DC during the soft-start, the inrush current limit is working, but slew rate is not controlled. After reaching 0.35V, slew rate control will start.
3. In case of LDO during the soft-start, the slew rate is controlled so it is <100mV/uV.
Regards,
Itoh