Other Parts Discussed in Thread: UCC2897A, UCC28084
I intend to use active clamp controller UCC289x for a stepup converter application. Input voltage 6V, input current <=20A, output voltage 24V nominal. I have a bias supply on board which provide 13.5V house keeping power for the UCC289x controller chip. My question is, is it practical to use P-mosfet as clamping switch? I am wondering the input voltage is only 6V, the aux drive output could go as low as GND, barely enough to drive the P-mosfet. N-mosfet will work for this application, but the more complicated driving circuit will likely take away the cost benefit, compare to a UCC2808x based push-pull topology circuit.
Compare to a push-pull converter for this step-up application, will active clamp forward topology provide much efficiency benefits?
Thank you. David