Dear Team,
Wanted to quickly check if we have a P2P drop in alternative to the LD39100PUR.
Thanks,
Needhu
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Team,
Wanted to quickly check if we have a P2P drop in alternative to the LD39100PUR.
Thanks,
Needhu
Needhu,
LP8340ILDX-ADJ/NOPB is p2p alternative.
LD39100 | LP8340 | |
AEC Q100 | YES | NO |
Output Options | Adjustable Output, Fixed Output | Adjustable Output, Fixed Output |
Iout (Max) (A) | 1 | 1 |
Vin (Max) (V) | 5.5 | 10 |
Vin (Min) (V) | 1.5 | 2.7 |
Vout (Max) (V) | 5.1 | 9.3 |
Vout (Min) (V) | 0.8 | 1.25 |
Fixed Output Options (V) | 1.2, 1.8, 2.5, 3, 3.3, ADJ | 1.8, 2.5, 3.3, 5 |
Enable | YES | NO |
Power Good | YES | NO |
Output Capacitor Type | Ceramic | Ceramic |
PSRR @ 100KHz (dB) | 45 | 10 |
Noise (uVrms) | 30 | 250 |
Accuracy (%) | 3 | 2 |
Vdo (Typ) (mV) | 200 | 540 |
Iq (Typ) (mA) | 0.02 | 0.019 |
Thermal Resistance θJA (°C/W) | 55 | 70 |
Min Package Area (mm2) | 9 | 9.6068 |
Package Type | SON | WSON |
Regards,
Prakash L
Hey Prakash,
Thank you Sir. Will write an email to you to align on something.
Thanks,
Needhu