Other Parts Discussed in Thread: LP8340,
Hi team,
custoemr need a very low Iq LDO in battery applicaiton, the spec as below:
input is 6.5V
output 3.3V
output current >500mA
they have evaluate the TPS7A26 and LP8340, they have below quesitons:
1. how about the efficiency of TPS7A26 and LP8340
2. any more better recommendation
3. if they use adjust version of TPS7A26, they want to increase the divider value to decrease power consumption, what't the maximum reisitor vaule.
thank you