Hello,
I'm looking for hints how to configure properly PFSM in TPS65941212EVM.
Assumptions:
-FSD is ignored (masked)
-First power mode is "Standby"
-Transition to "Active" only when ENABLE=HIGH
-Transition to "Standby" from "Active" is done when ENABLE=LOW
Enable pin is forced in low state by additional PD resistor added on EVM (so default state should be "Standby")
My configuration is following:




Unfortunately - after programming, when I'm pulling up ENABLE to 5V I can't observe transition to ACTIVE state (I'm checking LDOs/Bucks output)
I checked ACTIVE mode definition separately , by STARTUP_DEST register change to ACTIVE (after this LDOs/Buck are working, so I'm assuming that sequence/outputs are properly programmed).
Any idea what should be changed in PMIC config ?
BR,
Krzysztof