Part Number: BQ77915
Other Parts Discussed in Thread: BQ25798, BQ77905
Hi,
I am planning a design for a 4S LiFePO4 system using the BQ77915, in conjunction with the BQ25798 charger, in accordance with a recent suggestion.
I have been reviewing the datasheet for the BQ77915 and I have what seems like a pretty basic question, but i can't seem to find the answer in the datasheet - apologies if I am missing something obvious.
Table 9-1 of the datasheet lists various functionalities, and mentions for example, that the OV threshold is " 3 V to 4.575 V (25-mV step)". How are these thresholds programmed? The 7 devices variant available, that are listed in Table 6-1, do not cover this whole range in 25 mV steps.
I see mention of an internal EEPROM that stores the thresholds in several places in the datasheet, but there seems to be no way to program it. So, if one wants some slightly different values than one of the variants available, is it something that one specially requests?
Thanks,
Best regards,
Anand.