Part Number: TPS55340
Other Parts Discussed in Thread: TPS63060, TPS63070
Model: TPS55340PWPR
=> 2 lithium batteries, 6V drive
This time, Vout = 6V in accordance with the motor rating and required performance.
However, in case Vin = 6V or more (6.1V to 6.5V) at the initial (shipping) stage with two batteries, will there be a major problem with the IC operation?
If Vin = 6V or more (6.1V to 6.5V) at the initial battery stage (shipment) with two batteries, will there be any major problems with IC operation?