Other Parts Discussed in Thread: TPS3704, TPS3307
Hi,
I am looking for a voltage monitoring IC which can monitor all the power rails in the board. Monitoring is required to ensure rails applied to a given IC are valid before lifting reset.
Rails Requirements are as below:
Rail 1: 0.84V (Core)
Rail 2: 0.84V (IO)
Rail 3: 1.8V
Rail4: 3.3V
Please suggest a Monitoring IC for the same.