Other Parts Discussed in Thread: UCC21710
Hello.
I apply power input on VCC1(TP5) 5V and GND(J2:11) 0V, 5-0V PWM signal on IN+ and short TP11 with OC pin.
At one point during the evaluation, RDY led was turned off and there became no output.
I measured the value on pin of Gate Driver IC UCC21710 directly using Digital multimeter and the value was
RDY=38mV, FLT bar=1.8V, RST bar/EN=4V, VDD=16V, COM=0V, VEE=-5V
I think all the value is okay except RDY pin.
There seems to be no output after RDY output drops. I want to know if there is something wrong with the internal logic in RDY and if there is a solution.
Thank you.