This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Sir
Attatched the Pin 13 & Pin 14 's waveform .
The following 13 - and 14-pin theories should be complementary. Under what circumstances will the overlapping uncertain states in the figure appear?
Sch:
Hello,
I reviewed your schematic and you have setup voltage amplifier into a voltage follower configuration and have your own discrete feedback scheme.
So comp should be the same as EA+.
So COMP is demanding maximum duty cycle and drops to zero volts because your compensation network demands it. The A and B pulses are synchronized to the master clock. The duty cycle is controlled by phase shifting out C and D. When you demand 0% duty cycle the C and D pulses will be phase shifted from 180 degrees to zero degrees. This will make the C or D pulse look to be on/off for more than 50% duty cycle. This is what your waveforms are showing.
Regards,