Other Parts Discussed in Thread: BQ24170

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Hi,
Thanks for the clarification.
Few more queries:
1. Will BQ34110 Fuel gauge works with BQ24170 Battery charger?
or it has any specific pairing device.
2. If BQ34110 has any specific pairing device, could you suggest the device?
3. Is any standalone device driver available for BQ34110? and could you share it?
Hello Dharani,
In general, the bq34110 can work with any charger. If there are specific charger features that require something from the bq34110, then you will need to check if the commands are compatible.
I would recommend that you post charger questions on the battery charger forum.
Device drivers for bq34110 are similar to bq27xxx which are included in the Linux kernel