This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3410: Review of inductor selection

Part Number: LM3410

 I would like to use the LM3410 for powering a TFT Backlight Panel.

The backlight specifications are as following:

-  3 Strings of 6 LED each
- Total Rating: 16.2-19.8V @ 60mA

I used the part of 8.2.1.2.2 from the datasheet since its rather similar to my application, therefore

Dmax = (Vout - n x Vin) / Vout  =  19.2V - 0.9 x 5V = 0.76

and the Inductor:

L1 = (Vin x Dmax  x Ts) / 2x ILpp   = (5V * 0.76 * 625us) / 2 x 120mA = 9.6uH

For the inductor i would choose 12uH

The inductor of choice would be Coilcraft LPS6235-123MRC (12uH 20% 1.75A 110mOhms shielded)


Is this a good choice and  correct calculation