This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5035: Reference Design

Part Number: LM5035

Hello E2E Experts,

Good day.

I want to use the LM5035 controller for input voltage range 150Vdc to 350Vdc and output 24V/20A.

Design ref. given in the data-sheet is up to 75Vdc max.

Please let me know, Can I go for the design half-bridge converter with LM5035 for 150Vdc to 350Vdc input voltage range?

Regards,

CSC

  • Hello,

    Yes, you can use it for high voltage. But you need make some changes from reference design. Input voltage can't be directly connected VIN of LM5035. A regulator is required to regulate the input to right range for VIN; then you need add an external driver (high voltage LS/HS driver) to drive MOSFETs.  Other parts are the same.