Other Parts Discussed in Thread: TPS65982, TPS65987D
One of the options for VBUS is using the PP_HV1,2,3,4 inputs. These are tied to BOARD_12V via jumper J18. There doesn't seem to be an obvious way of getting 12V into the board ? Do we need to use an external power supply and use J18 as an input connection ?