Can the IADJ pin on the LM22673 be tied to ground?
What would happen if it was connected to ground?
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Can the IADJ pin on the LM22673 be tied to ground?
What would happen if it was connected to ground?
Thanks in advance.
Our circuit would see a max input of 16V and draw 0.5A at 3.3V, would that still cause damage if the IADJ pin was grounded?
Thanks in advance.
Hello
The damage would occur to the circuit that is connected to the IADJ pin to control the current limit.
Grounding this pin can cause excessive current in the current limit control circuit.
Are you trying to substitute the LM22673 for another device that has this pin grounded on the PCB ??
If you can give me more information I may be able to help further.
Thanks