Hi,
I got an issue with the REGN pin periodically dropping, with the charger chip also rebooting and losing all the configurations.
The REGN pin is driving nothing except for the VDDA pin and two resistors (100Kohm and 59Kohm) to set ILIM_HIZ. on the output there is a 2.2uF 16V ceramic capacitor. Derating with DC bias for 6V gives leaves me with 1.98uF
There is no way I am exceeding the 50-60mA current limit.
What else could be causing the regulator to be overloaded?