hi sir
I want to design a battery cell monitor, use BQ76952PFBR
1.Please help to check the circuit is right?, I only monitor the eight battery & 4 temp ,without over current/over voltage protect
2.REGIN(pin 36)apply +15v, the command the REG1 LDO 3.3V output, the circuit is right?
3.if I use the not used pin to monitor others voltage(not cell voltage), ok?
thanks