This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R2: LEDCNTRLA / LEDCNTRLB / LEDCNTRLC anode and cathode segments?

Part Number: BQ40Z50-R2
Other Parts Discussed in Thread: PMP, BQ40Z50

Hi,

In regard to circuit associated with BQ40Z50-R2's LEDCNTLA, LEDCNTLB and LEDCNTLC I am trying to understand the current flow through the LED's and therefore which segments constitute the anodes and which segments are the cathodes as upon evaluating the circuit diagram on pg 30 of the attached owners manual the input of one LED appears to be the outlet of others. For example the input line segment of LED3 / D2 appears to be the output line segment of LED4 / D4 and LED1 / D5. Any guidance that can be provided on how the current flows through the circuit associated with the LEDs would be greatly appreciated.


Best Regards,

Joe DeWitt PE, PMP

bq40z50-r2 Owners Manual.pdf