Can you please confirm that charge termination indication via tapper current, as described in section 3.7 of TRM is critical only for learning cycle?
I have 16 series cells with each cell 280Ah. My charging profile during normal operation will be CC/CV which essentially cuts off the current (almost step change from charging current to zero current) once desired pack voltage is reached. This means that under normal operation, end of charging profile will not meet requirement of taper current window. I need to make sure that it is ok for normal operation and battery guage performance will not be impacted. For learning cycle, I can force the profile required for charge termination indication since its just one time
Best regards
Fahad