Hello LP team,
Do we have a LDO which meets the below requirements?
- Vin=5.5~6.0V
- Vout=5.2V or 5.5V
- Iout=less than 150mA
- Current limit feature: 200~250mA
Best regards,
Shotaro
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello LP team,
Do we have a LDO which meets the below requirements?
- Vin=5.5~6.0V
- Vout=5.2V or 5.5V
- Iout=less than 150mA
- Current limit feature: 200~250mA
Best regards,
Shotaro
Hi Shotaro,
We don't have anything that meets those requirements specifically, but can you help me understand what your actual application need is? You are asking for an output of 5.2 to 5.5V, which is very uncommon, and the input voltage range that you specified won't support a 5.5V output unless you are at the 6V end of that range.
If you can help explain your application a little more maybe I can help find you a part that will work.
Mark