This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5121: CC/CV 2A 70V capacitor charger

Part Number: LM5121

I need to design a capacitor charger using a CC/CV boost converter with the following settings:

Vin = 24V, Vout(CV) = 70V, Iout (CC) = 2A

Is there any reference design using LM5121? is it the best choice?

Thanks,

RS