Other Parts Discussed in Thread: TPS546D24A,
Hi team,
The Table 8-2 recommends ILOOP=6 for 550kHz frequency.
But, calculating it from Eq. (26) in TPS546D24A datasheet, the result is 4.767,
which is same as TPSM8D6C24 typical application / EVM value.
Which do you recommend, 6 or 4?
Did this difference come from difference between TPS546D24A and TPSM8D6C24?
Also, how would I set VLOOP?
I tried to calculate with Eq. (10), but the digit of the result (5.288*10^(-6)) is too different.
⊿V_OUT=10 mV
⊿I_OUT=11.64 A
CSA=6.155 mV/A
N=2
VOUT_SCALE_LOOP=0.5
Could you let me know how to calculate it out?
Regards,
Itoh