This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPSM8D6C24: Compensation selection

Part Number: TPSM8D6C24
Other Parts Discussed in Thread: TPS546D24A,

Hi team,

The Table 8-2 recommends ILOOP=6 for 550kHz frequency.
But, calculating it from Eq. (26) in TPS546D24A datasheet, the result is 4.767,
which is same as TPSM8D6C24 typical application / EVM value.
Which do you recommend, 6 or 4?
Did this difference come from difference between TPS546D24A and TPSM8D6C24?

Also, how would I set VLOOP?
I tried to calculate with Eq. (10), but the digit of the result (5.288*10^(-6)) is too different.

⊿V_OUT=10 mV
⊿I_OUT=11.64 A
CSA=6.155 mV/A
N=2
VOUT_SCALE_LOOP=0.5

Could you let me know how to calculate it out?

Regards,
Itoh