Other Parts Discussed in Thread: LM5176
Hi
Please help suggest alternatives to LT8582
The conditions are as follows
Current Mode FB
The output voltage VPOS 15~17V , VNEG1 -13~-11V
Thank you
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
We do not have exact replacement for LT device you mentioned. The closest TI device with split rail output (+/- output) with the voltages you specified is TPS65131. Its datasheet is available online.
Kind Regards,
Liaqat
Hi Liaqat
If LTC is not used, the conditions are as follows: Input voltage 12V Switch to 2 voltages.
The first voltage is 12V input to 5V~27V output, (FB will be used to adjust the Output voltage) Output current max 3A.
second voltage 12V input to negative voltage -1V ~ -20V, (will use FB to adjust Output voltage) Output current Peak 3A.
Ps. It is better to be the solution above Dual Output.
Hello,
I am busy with some other customer support issues but will look into your query and get back to you by Monday my time (California).
Kind Regards,
Liaqat
Hi Gareth,
Unfortunately, I do not see a solution in our portfolio to meet these specs. Almost all of the devices in our product line are 3-6V input devices but let me assign this thread to a product line that has wider Vin devices and someone may respond with a possible solution.
Kind Regards,