This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi team,
We put a 12ohm resistor with a current meter in series to the Vout0 of the eval board. When we used the GUI (LP8758-xxEVM GUI — SNVC189.ZIP (6093KB)) to program the output voltage, the GUI read back much lower current. We got the same results after changing to different Vouts and even the 2nd eval board. We understand LP8758 has the resolution of current measurement as 20mA. Is this expected at low current scenario?
Programmed output voltage | Ideal current draw | Current reading from the current meter | Current reading from TI GUI |
1V | 83mA | 80mA | 0mA |
2V | 166mA | 160mA | 60mA |
Thank you,
Tony