Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.

This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61288: Using two in parallel

Part Number: TPS61288

Hi,

Is the boost support to connect two in parallel ? 

I would like like to use 12V/2A for output while my input is 3.3V.

I know that the device is support to use one with my requirement. but, I prefer to use two in order to reduce the temperature junction of the IC.