Team,
Can you help clarify worst case Pgood set and trip points for the TPS61378?
1. In the datasheet I see that Pgood sets at 90% but then has a 5% hysterisis. Does this mean after Pgood is high we need to be at 85% to drop low again. (Assuming 5V0 out then Vout would need to be 5.0*0.85=4.25V to drop)
2. The values in the datasheet are just shown as nominal, what are the min and max values for VPG_TH and VPG_HYS:
Best,
David