This time, two types of voltages are supplied to the VCC and MPPSET pins of the BQ24650RVAR on the same circuit.
Two types means that there are two different power supplies.
One is the main power supply, 17.4V, and the other is the secondary power supply, 12V.
Since 17.4V is the main power supply, R3 and R4 are selected with VMPPSET as 17.4V.
However, in this case, when the power supply is changed to the secondary power supply, the voltage to the MPPSET pin will be 12V, so the voltage to the MPPSET pin will be less than 1.2V due to resistive voltage divider by R3 and R4, and the charging current to the rechargeable battery will be reduced.
In order not to reduce the charging current even when the secondary power supply is used, is there a problem with supplying 3.3V to the MPPSET pin and keeping it active at all times when the secondary power supply is used?
Regards,
Kagawa