Hello Team,
The TPS272C45D is used in a setting where VOUT > VS in some cases, which leads to an inverse current through the MOSFET body diode. There is no specification in the data sheet regarding the maximum reverse current. For example the datasheet for the TPS4H160 specifies the reverse current IR(1) and IR(2). Is it possible that you make a similar specification of the maximum reverse current for the TPS272C45D?
Thanks and Best Regards, Hans