If Iout is changed to higher value than 0.06A the design calculation is not possible. But the device should be able to deliver 0.68A
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
If Iout is changed to higher value than 0.06A the design calculation is not possible. But the device should be able to deliver 0.68A
That is exactly my problem. It does not matter which input voltage and output voltage is used. It is never possible to set more than 0.06A Iout.
Or in other words: At which condition can I set 0.07A? Or even 0.68A? It is simply not possible. Never.
Hi Alge,
I entered the input voltage 4-4.5V, output voltage 12V, Iout 0.1A. The WEBENCH could generate the design.