Hi support,
For TPS74701 implemented in one project, we have below configuration:
Input Voltage & BIAS voltage: 3.3 V connected together;
Output Voltage: 1.1 V
Current: 0.4 A
The 1uF input capacitor is near BIAS pin, there is no input capacitor near VIN pins.
What is the impact of using 1uF? stability issue, noise issue, reliability issue?
The datasheet recommends minimum 4.7uF input capacitance when Vin and BIAS are connected together.
Thanks,
Wei