Other Parts Discussed in Thread: TPS7A47
I am working on a design which uses TPS7A3301 for generating -2.5V output using an input which can go till -6V. One of the requirements I have is to drive the output pin externally using another supply to -2.6V for a small duration and then bring it back to its normal state. These are the following questions:
1. For the above condition, if I configure the device to output -2.5V but force output to -2.6V, is it expected to damage the device?
2. In case there is a chance of device damage, will pulling the "EN" pin put the output in a high-Z state and prevent damage to the device?
Note that when I am forcing the output externally, I plan to keep the input held at -3V (for both 1. and 2.)
(I have a similar query for TPS7A4701 where I plan to force output voltage to 2.6V using an external supply when the device is configured to output 2.5V in normal situation)