I am using TI BQ34Z100-G1 EVM which can only support upto 2A of current. I need to do learning cycle, but my cell capacity is greater than 100Ah. This means using the EVM, my discharge current will be less than minimum recommended value of C/10. TRM says that resistance tables will not be updated if discharge current is low, my question is how critical it is to update resistance table for guaging performance assuming everything else in the learning cycle goes as recommended?
FYI, for now I am only testing the guage operation with EVM, for actual product we will offcourse redeisgn the board to suppprt higher amp
Best regards
Fahad