Other Parts Discussed in Thread: TIDA-010015, UCC24624, , UCC28064A
Hi team,
my customer has a very strict power saving spec at tiny load (120mW, 24Vout)
they're using TIDA-010015, and the measurement result Pin is 296mW, which is 10mW above their spec,
While I was looking where can I improve the power loss,
I notice the standby current of UCC24612 is much higher than UCC24624's,
May I know how much current can we save if we use UCC24624 to replace two UCC24612 in VDD "24V" ( since datasheet only has 5V and 12V)
please give me a range (min and max)
thanks