Hello,
Customer wonder to use this device in MD sector. Here there are few questions. please help to support.
1. Is these any method to control the current limit of the device? on the datasheet, the variation of the current limit is from 6.3A to 9.5 at certain conditions. But customer would like to know if they would like to control the max. limit current from 9.5A to 8.5A for an instant. is there any way to do? how about to pull a zener diode to clamp the Voltage at VCOM pin?
2. It seems there is no over current waveform on the datasheet? In the d/s, it says it's using foldback frequency against the short and over current. But why it says the output overload conditions reset the soft-start timer? what's this purpose?
During the foldback freq. event, Is output rail able to delivery current to the output continuously? What's the difference between the Foldback and hiccup mode during short fault condition?
Regards
Brian W