Other Parts Discussed in Thread: BQ24650
The default current setting of BQ24650 Development board was 2A i tried to increase it to 8A by changing the following.
1. Inductor of 3.3uH
2 . Output capacitor(C2,C1,C7) , 10V,10uF , 4 connected in parallel value comes to about 36 uF.
3. R6 resisitor R005, 0.005 ohm.
Still it is able to handle 4A max. How to increase ?
Thanks and Regards
Akanksha