This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM34927: LM34927 replacement part

Guru 12795 points
Part Number: LM34927
Other Parts Discussed in Thread: LM34926, LM5017, LM5018, LM5161

Hi,

I am using the WSON package of LM34927. From the viewpoint of IC availability, we are considering replacement with P2P.
Is it okay to assume that all of the following devices will be replaced by P2P? Please let me know if there is a difference other than the current limit value.

・ LM34926
・ LM5017
・ LM5018
・ LM5161

The conditions of use are as follows.
・ Vin: 15-96V (for use in both 24-input system and 48-input system)
・ Vout1: 13.5V, Vout2: 13.5V
・ Iout1: 100-150mA, Iout2: 100-150mA

Thanks,

Astro