Hi,
When repeatedly charging and discharging, the value of RSOC is observed to gradually increase abnormally, and when the Scale Factor setting in Current Scaling is changed, the RSOC value shows a stable behavior.
Please refer to the attached file for more detail.
The specifications of the battery pack include
- Maximum charge and discharge current 180A
- Current detection resistance 0.1mΩ
I believe there may be a problem with the Scale Factor setting value. Please advise the cause of this and the correct solution. Please let me know the appropriate Scale Factor setting value.
Best regards,
Sato